Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Slide 33
Product List
There are several industrial standards defining robustness against electrostatic discharges. The most important and well known is the IEC61000-4-2 standard, which defines a measurement setup that simulates everyday ESD strikes very well. This standard defines four levels of ESD robustness, from 2kV up to 8kV, that an ESD protection device has to be capable of withstanding. In the standard IEC61000-4-5, the voltage pulse has a rise time of 8µs and fall time of 20µs defined. With the help of this defined pulse, the capability of withstanding current and power surges is defined. For both of these standards, the whole system is tested, which at least consists of the protection device and the circuit to be protected circuit. The MIL-883E standard, on the other hand, only tests the ESD robustness of the device itself. The “machine model” and the “charged device model” are not commonly used.
PTM Published on: 2011-11-02