Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
protection vcl
The clamping voltage (VCl) is sometimes a disregarded electrical parameter for protection devices, but one of the most important. It specifies the maximum voltage drop across the protection diode during an ESD strike; this is the same voltage drop that will occur across the protected circuit. It therefore has to be below the maximum allowed voltage drop of the protected circuit to guarantee that it will not suffer damage.
PTM Published on: 2011-11-02