Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Slide 33
Product List
In summary, voltage can be generated by friction between objects and can reach very high levels - up to 35,000 volts from walking across a carpet, for instance. When this energy potential is suddenly discharged into an unprotected electronic device, there is a high potential for damage which could render the device inoperable. Additionally, if these ESD strikes are not properly protected against, the probability of increased warranty cost, a lowered customer satisfaction, and damage of the brand name is largely increased. To protect electronic devices from potential ESD damage, Nexperia offers a broad range of devices in various packages. Nexperia also offers several internet resources to aid in the design process which utilizes these ESD protection devices including datasheets, a selection guide, application notes, spice models, and a cross-reference tool.
PTM Published on: 2011-11-02