Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 4
The feature-rich F990 devices enable an extension of battery life with an MCU that enables a wake-on-touch solution and the low power sensing of the F990 family. The hardware CDC provides exceptional levels of SNR, typically near one hundred, resulting in highly responsive touch sensing even in noisy environments. Available in a tiny 3x3 mm package, the F990 accomplishes this with no external components, yet offers additional integration of commonly used hardware peripherals such as the high performance ADC, current DAC, and digital functions such as timers and PWMs. Finally, QuickSense™ Studio enables the rapid deployment of touch sensing solutions to reduce time to market.
PTM Published on: 2012-05-16