Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Product List
The space savings are even greater for high pin count devices, such as for a 56 pin device. A leadless replacement to an SOT371 can bring up to 82% of PCB space savings by utilizing a modified pin-out. The SOT1033 shown here uses a double row of pins along all four sides of the package, as opposed to a single row of pins on just two sides of the package. This simple technique drastically reduces the package footprint.
PTM Published on: 2011-11-02