Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
Cyclone-Slide25

Further power consumption control is provided to the user by allowing them to shut down the transceivers, PCIe hard IP, and supporting circuitry to minimize power consumption when not used. Quartus® II will automatically power down unused transceivers and the user can dynamically power down any of the sub-blocks available through the signals listed in the table on this slide. It should be noted that there will be a leakage current for the “powered down” blocks which will be an order of magnitude lower than the operating current.

PTM Published on: 2012-05-29