Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Product List
This table shows the various Hall ICs that ROHM offers. Omnipolar detection Hall ICs can detect both S-and N-pole magnetic fields, simplifying magnet management. Omnipolar Detection Hall IC with polarity discrimination includes a polarity determination circuit that enables operation (output) on both the S- and N-poles, with the polarity judgment based on the output processing configuration. This Hall IC product can be in applications involving crystal panels to detect the front-back location or to determine the rotational direction of the product. Unipolar Hall IC detects only N pole. Unipolar sensors can be in doors, covers, and other applications in order to detect open and close of the object. Bipolar Latch Hall IC detects polarity change for both S and N pole. The operation is more stable compared to magnetic force detection, as the duty on output pulse will be consistent.
PTM Published on: 2018-06-25