Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
VIC
System controls for the LPC2300 and LPC2400 MCU families feature the Vectored Interrupt Controller, the Phase Locked Loop, Power-On Reset, Brown-Out Detect, various power down modes, emulation, and debugging. The ARM7 core only has two interrupt inputs so the LPC2300 and LPC2400 have added a Vectored Interrupt Controller (VIC) which assigns up to thirty-two interrupts with sixteen levels of prioritization. Additionally, each peripheral has one dedicated interrupt line connected to the VIC with multiple flags and various sources. With these MCUs, any pin on PORT0 and PORT2 can generate an input, therefore granting flexibility to tailor interrupts for each application.
PTM Published on: 2011-11-02