Flash is one of the key differentiating elements of the NXP microcontrollers and is an important factor in the huge success of the family. The NXP Flash is the highest performing flash available on an ARM7 microcontroller, performing 37% to 51% faster than its competitors. This is because NXP’s Flash has the ability to execute code at frequencies up to 72 MHz with zero wait states.