Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Product List
The EVE / FT800 documentation is available through the FTDI website. Links to various guides, application notes, and data sheets are noted above. In addition to the FT800 IC itself, FTDI also produces complete HMI interface solutions complete with LCD, touchscreen and amplified audio. The VM800C “credit card” sized development system allows for quick prototyping while the VM800B mounts all of the components in a production-ready bezel. Be sure to check the EVE pages on the FTDI website for new application notes, sample code, and EVE products. Additionally, make sure to check out FTDI’s YouTube channel to see numerous examples of displays that can be created with EVE technology. In addition there are 3 utilities that are discussed for audio, images, and fonts that can be utilized to easily create user specific items for the EVE environment.
PTM Published on: 2013-10-02