Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Product List
The modules come with a full AT command based software stack. Within that, the software package will give users a .bin file that can be downloaded to the module direct via UART, an .ota file, which is a slightly different configuration that can be downloaded over the air, and the change logs and license file. There are two different versions: the 001 is for the .11 family and the 002 software package is for the .21 family, so users will want to make sure they load the proper firmware package.
PTM Published on: 2016-02-01