Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
Smart Grid Solutions: Smart Grid Distribution/Smart Meters Slide 6

The main components of the Smart Grid are shown on this slide. Sensors and controls provide information on the status of the grid and the ability to make changes. Two –way communications between grid operators, components, and consumers help utilities run the grid, and help consumers manage their energy use. The Smart Grid will require improved hardware and software resources, data will need to be analyzed and acted upon in real time. Security of data and Smart Grid components will also need to be considered. Therefore, there will be increasing requirement for applications and information technology. Consumer and end-user electronic devices enable consumers to manage their energy use, and allow the utilities to manage peak demand and load.

PTM Published on: 2013-08-23