Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Image of MoSys Accelerator Bandwidth Engine: High Performance/High Bandwidth - Blazar Family Architecture

The Blazar family of products is made up of three main products: the BE2, BE3 and PHE. The BE2 is comprised of 576Mb of memory with two GCI ports to access the device, each with SerDes interface speeds up to 12.5Gbps, a tRC as low as 3.2ns, and an interface bandwidth of up to 320Gbps. The BE3 is comprised of 1.1Gb of memory with two GCI ports to access the device, each with SerDes interface speeds up to 25Gbps, a tRC as low as 2.7ns, and an interface bandwidth of up to 640Gbps. As part of the support that Peraso offers with Blazar, Peraso has options to supply sample RTL code for the memory controllers or, for a small fee, Peraso can support the development of a controller for the environment (FPGA and version of a tool) that is being utilized.

PTM Published on: 2021-08-11