Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
FlashCards-slide11

Given the varying cost-per-capacity ($/GB) for different NAND Flash memory, it is essential to perform a TCO analysis specific to the application and usable life requirements. In general cost/capacity is highest for SLC, followed by aMLC, MLC and finally TLC NAND Flash memory. However, endurance ratings and effective usable life also greatly varies between these NAND Flash memory types. An estimation in terms of cost/terabytes written ($/TBW) provides a more accurate metric for selecting the type of NAND Flash memory. Analyzing as a whole, variables including NAND Flash media capacity, number of years of usable life, DWPD and cost will help the user determine the right choice of media.

PTM Published on: 2015-10-20