Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Product List
Some Toshiba load switch ICs include reverse current blocking. Unlike MOSFETs, which can suffer from significant leakage through the body diode, load switch ICs are able to stop reverse current flow when the switch is reverse biased. This is very useful in cases where there are multiple power sources and the designer wants power to flow only in one direction.
PTM Published on: 2013-07-26
PTM Updated on: 2017-07-10