Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Product List
Load switch ICs have a safety feature that turns off when temperatures exceed the chip’s junction temperature. A temperature circuit is built into the IC itself, and follows a hysteresis curve, turning off at 150°C and turning back on again at 85°C, approximately.
PTM Published on: 2013-07-26
PTM Updated on: 2017-07-10