Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
lineup
The RX651/RX65N group is the newest addition to the RX600 series, featuring a 120 MHz second generation RXv2 proprietary CPU core, developed in a high performance, low power 40 nm process. RX65N adds a 100 Mbps Ethernet controller, and RX651 is the version without Ethernet. The RX600 series MCUs also combine fast interrupt response, safety features, and an efficient bus architecture that boosts system performance.
PTM Published on: 2018-03-06