Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Product List
Renesas is introducing several exciting kits based on RX65x high-density products. First, the Renesas Starter Kit (RSK) is designed to enable customers to test the full set of features in RX65x. Just as a side note, there is an RSK available for each RX MCU in production. Renesas is also pleased to offer two low cost kits to enable broader market adoption. The Envision Kit comes with a WQVGA TFT display, and includes several demos, highlighting both the HMI features as well as on-the-fly flash firmware updates. The kit also includes a built in E2 Lite on-chip debugger and a quick start guide. The Target Board for RX65N is a low cost kit with footprints for an optional 100-pin header and a PMOD, ready for a variety of applications. The kit also includes a built in E2 Lite on-chip debugger, avoiding the need to purchase one separately. All three kits are designed to help customers get their RX65x-based applications up and running quickly.
PTM Published on: 2018-03-06