Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 19
When the microcontroller first powers on or wakes up from Deep Sleep, it will start executing code from the Reset vector. If the RTCC is using the secondary oscillator to keep track of time, the secondary oscillator should be enabled before clearing the Deep Sleep release bit. This allows the RTCC to continue operating continuously, without losing time. Deep Sleep hardware will keep the RTCC and secondary oscillator running throughout Deep Sleep and wake-up, but firmware needs to re-enable the RTCC on wake-up so that the module doesn’t get disabled when the Deep Sleep release state bit is cleared. Applications that are not using the real-time clock can skip this step.
PTM Published on: 2011-10-28