Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Product List
Deep Sleep is great for applications that are inactive for long periods of time, such as remote controls, input devices, sensors and thermometers. It is also ideal for applications that need to keep accurate time while consuming minimum power because Deep Sleep supports continuous operation of the Real-Time Clock/Calendar where desired. The longer an application can stay in Deep Sleep mode, the lower the average current consumption of the device will be. Normal Sleep mode is recommended for applications that need ultrafast wake up times, complete state retention, or will only be inactive for short periods of time.
PTM Published on: 2011-10-28