Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Product List
Associated Content
Clock generators are integrated circuits (ICs) that generate multiple output frequencies from a single input reference frequency. The input or reference frequency is supplied by a crystal, XO or other clock in the system. Clock generators may have other features that can be controlled by I2C or pins such as: turning on/off outputs, skewing frequencies, and adding/removing spread spectrum to frequencies to reduce noise. The perceived challenge with clock generators is system layout. Placing a crystal adjacent to its target IC is simple and cheap. Routing a clock signal from a clock generator to its target IC might not always be as easy, although it can save money. Careful design and other techniques can ensure a centralized clock source provides equal performance. Generally speaking, if four or more clocks are required designers can save money with a clock generator.
PTM Published on: 2017-03-01