Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
best fit
RX is the broadest 32-bit family in the market, fit for almost every application. Special features are available for many applications like Human Machine Interface (HMI), where a WQVGA TFT display can be driven by the internal TFT controller without the need for external RAM for the frame buffer. Another application is motor control, where the unique timers and performance can drive up to three motors.
PTM Published on: 2018-04-09