Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Product List
The RX family of microcontrollers delivers superior performance in terms of core processing performance, code efficiency and power consumption. An extensive portfolio of on-chip mixed-signal peripherals is available, and fast Flash memory is embedded. That Flash unleashes full CPU performance, feeding instructions to the 32-bit RX CPU with no delays – no waits, no stalls – maintaining the MCU’s peak performance at 1044 CoreMark. Using RX MCUs results in a pure, predictable performance in the design with a vast amount of benefits. Thanks to the Renesas process technologies, the RX core shows the full performance in a very power efficient way. Ready-to-use solutions for motor control, capacitive touch, HMI, industrial networks, industrial and home appliance safety, and many more, enable a quick time to market.
PTM Published on: 2018-04-09