Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
rx 32bit
The RX family has four members, targeting different performance ranges. The RX100 runs at 32 MHz and the RX200 up to 80 MHz. Both are using the same 130 nm low power process technology, enabling 5.5 V operation and very EMV robust designs. The RX600 runs up to 120 MHz, the same speed the Flash achieves, and the RX700 runs up to 240 MHz. Both have one communality. This is again the process technology. A performance and low power in active mode optimized 40 nm technology.
PTM Published on: 2018-04-09