Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Slide 59 Slide 60 Slide 61 Slide 62 Slide 63 Slide 64 Slide 65 Slide 66 Slide 67 Slide 68 Slide 69 Slide 70 Product List
Electromagnetic Noise Reduction Slide 34

Our first recommendation is to try to reduce unwanted emissions from the oscillation circuit for the main clock that drives the microcontroller and other ICs in your system. Generally speaking, EMI levels grow as the clock speed rises. Noise from harmonic components can be inductively coupled within adjacent circuit patterns. Also, that noise is radiated through package leads and circuit board patters by antenna effects. To minimize these problems, review the oscillation constant and use as slow a clock frequency as you can. Also, examine the output of the oscillator at the normal supply voltage, as well as the extremes of the operating voltage range. If you find signal distortion, change the values of the components in the oscillation circuit to smooth out the output and eliminate overshoot and undershoot. For example, in the circuit shown here, adjust C1, C2, and R2.

PTM Published on: 2011-11-02