The BLE component simplifies the Bluetooth Low Energy stack and profile configuration. What would typically require many lines of code can now be done in a simple, intuitive, easy-to-use graphical user interface. The BLE component in PSoC Creator contains the Bluetooth 4.1 specification and the BLE Protocol Stack, including all of the supporting BLE Profiles, and has easy-to-use APIs for firmware development. As mentioned previously, the user can right click the BLE component in PSoC Creator to open its configuration tool. In the screenshot shown on this slide, taken in the profiles tab, profiles are included for a heart rate measurement which can be selected and used to set up the various parameters for configuration of the protocol Stack and the profile.