Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Product List
In summary, the Microchip AT86RF232 2.4GHz RF transceiver has been designed for cost-sensitive consumer applications. It offers excellent RF performance, along with very low power consumption. Operation at full performance is guaranteed down to 1.8V. It also offers important features such as antenna diversity. For easy evaluation, rapid prototyping and efficient development of wireless applications using the AT86RF232, the designer can use the Microchip ATREB232ED-EK Evaluation Kit and visit www.atmel.com/wireless to get the latest software updates.
PTM Published on: 2012-01-09