Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
eZ430 Development Tool Overview Slide 11

Because the Chronos features a wireless radio, the user has nearly endless possibilities on what can be controlled or what can be interfaced to. It will act as a central hub for just about any system that can be wirelessly enabled. That can be a heart rate monitor or a pedometer when going for a run. If the user has an integrated home with motorized blinds or electronic ceiling fan as an example, it can be controlled directly from the Chronos watch. Another example is a wireless transceiver inside a thermostat, which shows how hot it is in the house, and if it was too hot or too cold, the user can change that directly from the wrist watch. Using the PC automation functionality, the user can even control an entire entertainment system or home media server that is setup on a computer. The Chronos is very flexible on what it can communicate with.

PTM Published on: 2011-07-05