Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
MOSFETs-Slide9

This slide illustrates the quick cross-reference using the parameters previously mentioned, such as breakdown voltage, Rds(on), total gate charge, and the package. For instance, a competitor’s device which is easy to cross-reference because the Rds(on) is shown in the part number. In this case, the IPP60R1906 is 600V, the Rds(on) is under 190m, the gate charge is 63nC, and the package is a TO-220. The cross-reference in this case should be ST’s STP24N60M2, which is a 600V, 190m, 29nC device, in TO-220 package. The second example crosses the BSC011N03LS, a 30V, 1.1m max. with a 72nC total gate charge. The package is the TDSON-8, which is the equivalent of the PowerFLAT. In this case, the STMicroelectronics cross will be the STL220N3LLH7, which is a 1.1m max. device. As can be seen it is an easy exercise. ST also offers some tools that can help when doing the cross-reference in real-time, these are discussed later in this tutorial.

PTM Published on: 2017-06-02