Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
MOSFETs-Slide11

This slide compares the figure of merit (RDS(on) x Gate charge) for ST’s F7 technology and two main competitors, for a generic 100V specification. In this case, thanks to the lower RDS(on) of the ST technology, the lowest figure of merit is determined to be ST’s. F7 technology is a technology that operates from 40V up to 150V.

PTM Published on: 2017-06-02