Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Slide 23
Slide 24
Slide 25
Slide 26
Slide 27
Slide 28
Slide 29
Slide 30
Slide 31
Slide 32
Slide 33
Slide 34
Slide 35
Slide 36
Slide 37
Slide 38
Slide 39
Product List
Since FTDI devices enumerate as a custom class, they need specific drivers to be installed on the PC. In conjunction with the USB device ICs, FTDI provides a complete, royalty-free solution of device drivers at the application and bus layers. An RS232 serial port application can be used without modification and by just using the VCP driver. The VCP driver causes the USB device to appear as an additional COM port available to the PC. Application software can access the USB device in the same way as it would access a standard COM port. The VCP driver is used in conjunction with the FTDI D2XX bus driver.
PTM Published on: 2011-05-26