Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide18

Shown here from comparison to this same rating snap-in capacitor, it is down to less than 5% capacitance at –40°C and 10kHz. The snap-in’s –55°C, 120Hz capacitance would be down to less than 60% versus the more than 90% for the MLP.

PTM Published on: 2013-02-07