Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide2

In today’s high availability and high power environments, systems need to run with no downtime and on very high currents. If a component of this system fails it will need to be replaced without any interruption of the system. Some devices may have high load currents and/or large capacitors which demand high inrush currents on power up leading to large voltage and current transients on the backplane. These transients can be responsible for interrupting adjacent cards on the system.

PTM Published on: 2008-04-29