Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
HotSwap-Slide19

The layout of the MOSFET is very important as it will be the main power switch and may therefore be required to dissipate a substantial amount of power. An incorrect layout may result in the MOSFET overheating and damage or destruction. The expected worst case power should be calculated before when selecting the TIMER capacitor. Using this data and power/thermal derating data from the datasheet, a safe maximum temperature should be designed for worst case conditions. Additional heatsinks should be used where necessary.

PTM Published on: 2008-04-29