Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Power Inductor Basics Slide 4

As seen in the last slide, power supplies typically contain multiple magnetic components working in concert to achieve efficient power conversion, the required operating frequency, and the desired impedance. Here is a brief overview of the primary uses of inductors in power supplies. First, as a circuit filter or choke - Inductors are commonly used to filter or choke (attenuate or cut) unwanted noise out of a circuit by choking high frequencies and alternating current and allowing lower frequencies and direct current to pass. Second, for resonant circuits or frequency tuning - Inductors are one of the three primary passive components of a resonant circuit (R-C-L). Resonant circuits are a very important building block in many electrical circuits, as they enable the designer to “tune” the circuit and operate within a specific frequency range. Third, for energy storage - Inductors are used to store and release energy from their magnetic field.  Last, for impedance matching – Inductors can also be used to help match source and load impedance. Maximum power transfer efficiency is achieved when the impedance of a load is equal to the impedance of the source.

PTM Published on: 2012-12-06