Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Capacitive Touch Sensing Solutions Slide 41

The information on this page summarizes the key advantages of the family including their very low power consumption and the fact that all the algorithms are embedded because it is a Finite State Machine. Also, the newer generation of products provide even higher sensitivity, better filtering, and the built-in ratio-metric engine. There are two key differentiators of these devices when they are compared to the competition: built-in PWM controllers and a separate bank of the GPIOs and I/Os that can also be independently configured to be the sensing channel or GPIO.

PTM Published on: 2011-12-12