Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
74aup2g57
Shown on this slide are examples of dual configurable logic device applications. The 74AUP2G57 integrates two functions, allowing the configuration of many different combinations of logic gates. For example as a 74AUP2G0804 which combines a 2-input AND gate with a single inverter. Or as a 74AUP2G0208 which combines a 2-input NOR gate with a 2-input AND gate.
PTM Published on: 2015-04-14