Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Product List
There are several families with integrated Ethernet MAC/PHY as well as LCD drivers in 64 ~ 80 pin packages supporting up to 192 pixels. The LCD module even enables voltage contrast control with an internal boost capability. The superset device, PIC18F87J93, is an 80-pin part that includes 128KB Flash memory, 4KB of data RAM, and peripherals including a 12-bit ADC and CTMU for cap touch buttons. The Full-Speed USB families have program flash ranging from 16KB ~ 128KB and 28 ~ 80 pins. The 64/80 pin PIC18F87J50 includes USB support with a rich set of peripherals. In 28/44 pin packages, the PIC18F46J50 USB family supports 16 ~ 64 KB Flash with XLP low power and Peripheral Pin Select for mapping peripherals to the desired pins. Additional details on a few of these families follow on the next few slides.
PTM Published on: 2011-10-28