Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
snap-switch-slide3

The ZM series has three models:  ZM, ZMA, and ZMS. The ZM and ZMA are the non-sealed version while the ZMS is sealed with an IP67 approval when used with the potted wire leads. The ZMS also has a high and low over travel design that limits the plunger travel to give the designer’s application longer mechanical life if required.

PTM Published on: 2011-10-20