Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
snap-switch-slide14

There are many applications for the new series of switches. In addition to the typical ON/OFF switch application, the switches can be used to detect or sense if units are in place before the customer can activate their equipment. Shown here is a typical application highlighting the use of the LCA in a central vacuum system that will detect when the hose is inserted or removed from the wall outlet.

PTM Published on: 2011-10-20