Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
snap-switch-slide10

The LCS series is available with solder terminals, Quick Connect, PC configurations and wire leads. It is IP67 approved with the potted wire lead option and has an electrical rating of 6 amp @ 125VAC and an ENEC international rating of 3(1) amp @ 250VAC. The LCS is sealed so it is ideal in harsh or dusty environments, or environments where airborne contamination will cause reductions in switch life.

PTM Published on: 2011-10-20