The SAMA5D3 is a great fit for both user interface and networking applications. It offers processing power and bandwidth as well as an impressive number of communication peripherals. For “imaging and terminals” the SAMA5D3 has a unique value proposition because of the ISI peripheral and the performance of the Floating Point Unit. This is better than the competition that does not have a CMOS sensor interface and exhibits lower performance in FPU. This performance can be explained because the ARM® Cortex™-A8 is provided with FPU v3 while ARM® Cortex™-A5 features FPU v4. The SAMA5D3 is great for scanner applications which use both CMOS sensor and floating point calculation. With its low-power figures, the SAMA5D3 devices offer new possibilities for this class of device, it is a good solution for wearable computing applications.