制造商零件编号 3785
POE SPLITTER WITH MICROUSB PLUG
Adafruit Industries LLC
License: See Original Project Programmers Circuit Playground Raspberry Pi SBC
Courtesy of Adafruit
Guide by Chris Daly
Overview
To make a long story short, several years ago I ran out of space for electronics projects on my desk, and I looked to the wall as a new frontier.
In previous decades, I had spent a lot of time building computer systems in large metal "tower" cases. With the advent of hacker board computers like Arduino, BeagleBone, Raspberry Pi, and others it has become possible to assemble computer systems that are so light, they hang on the wall. So that's what I did.
My first few attempts were pretty clunky, as shown above. I would first assemble a functional computer system on a plastic base with a grid of mounting holes. Then, when I decided the system was basically working I would fit the plastic base into a wall-hanging frame.
Later I started to think about designing characters and scenes on the canvas. I had sometimes seen collage-style wall-hanging art incorporating non-functional parts, like chips, wires, connectors, etc. But I had never seen wall-hanging art that used functional computer systems, so I decided to delve into that niche.
You can find more information about the projects pictured here in my GitHub repos, like GuitarThing, ShipsAtSea, and fold.
At one point I thought ... what about a Kickstarter? Can this thing be scaled up? Will big manufacturers like Lenovo or Apple wake up and realize the wall is the new frontier for computing? (Nest is one answer to that.)
I ruled out a crowd-funded project. Overall, I don't really want to be involved in a manufacturing operation. What I enjoy most is designing each new system in some way different than what I've done before.
The process of thinking about scaling up the operation also caused me to reconsider the basic concept of computers on the wall and try to distill it to its most fundamental essence. For example, I wondered what is the minimal viable wall-hanging canvas enclosure computer system that could be easily assembled and shipped in quantity? I named my answer to that question the CompuCanvas model A0.
Here are some of the design ideas and lessons learned that guided the 'CompuCanvas' concept:
Even with constraints like outlined above, there are a multitude of possibilities. And these rules may be bent or broken as necessary to achieve even more.
Over time I've experimented with a lot of different parts and arrangements, but I still have barely scratched the surface of ideas.
For this guide, I'll walk you through the process of constructing a CompuCanvas type system. I will present a primary path you can follow as well as some alternate routes you may explore.
We'll start by creating a plain enclosure style CompuCanvas housing a Raspberry Pi 3B and a speaker, as shown below.
After that I will look at several variations on placing lights inside the canvas. One example of this is shown below.
Finally, I'll show how to make USB transitions to the front of the canvas to add external features with illumination.
Parts and Tools
This page is a master list of the parts and tools used in the guide. Some pages of the guide present optional paths that you may choose to skip, so you may not need every part shown below.
I'll start with the most essential parts from Adafruit. The CompuCanvas we build will house a Raspberry Pi model 3B with a USB speaker and a Power over Ethernet module. It will also use USB connected CircuitPython devices to create a light show on the canvas. These key parts are listed just below.
Note: For the other end of the Power over Ethernet splitter shown above, you will need an IEEE 802.3af compliant PoE 'injector', which takes power and Ethernet as input and will send them over an Ethernet cable to the PoE splitter shown above. The PoE injector part will be shown in more detail in upcoming sections of this guide.
Below are a number of additional parts from Adafruit used in this guide. Some of these are optional, as indicated in the description text.
Optional Lighting Parts
Cables
I have indicated a quantity of 2 for some of these cables below, but you may only need one depending on which of the interior and exterior lighting options you choose.
Tools
This guide uses some common tools that you can find at a hardware store, or maybe already have:
And here are a few additional tools used in the guide that can be found in the Adafruit store:
Art and Hardware Store Parts
Some of the parts you will need aren't available from Adafruit but should be easy to find at an art supply store and/or a hardware store. These will be covered in full detail in the next section:
Canvas Enclosure Parts
To get started on a CompuCanvas, you will need a few parts that are probably most easily found at an art supply store. In my area, we have Michaels, which is where I bought the parts shown here. I wasn't able to find URLs for the exact parts I bought, so I will show and describe them here. I think you will be able to find similar parts at an art supply store in your area or online.
Perhaps the most essential part for a CompuCanvas is the canvas! For this project, I recommend an 11x14 inch "Heavy Duty" style art canvas. You could probably make it work with a 9x12 inch canvas or go bigger with something like a 12x16 inch canvas and have more room to spread things out. (PyRulers for scale.)
Many of the art canvases I've seen are very shallow in the back - maybe half an inch - which is not a lot of room to work with. I have found some canvases labeled "Heavy Duty", which seems to designate a deeper design with about 1.5 inches of room to work with behind the canvas. I like to place USB speakers behind the canvas (so you hear, but don't see them), and the standard, shallow canvases would not have enough room in back for any USB speaker I've found.
Besides the canvas, there are two other essential parts for building this type of enclosure. The hanging wire and "D-ring hangers" shown here will allow for hanging the CompuCanvas assembly on a hook or nail in the wall.
The above parts are all you really need for a basic CompuCanvas enclosure. But for a more deluxe build, try to find foam board, like the 8x10 inch pieces shown here, and these 0.25 inch "offset clips". The offset clips will be used to hold the foam board in place behind the canvas. When designing a look for the canvas and laying out the electronic parts and cables, you may find that it works better to attach some parts to the foam board, instead of the canvas.
Preparing the Canvas
Before setting any computer parts on the canvas, I prepare the back, so it can hang on the wall. These art canvases come wrapped in plastic and I recommend leaving most of the plastic wrap on at this stage to protect the front of the canvas. As you will see below, I'll cut part of the plastic wrap in the back to allow for attaching the D-ring hangers and the (optional) offset clips for the foam board backing.
In addition to the parts shown in the previous section, we will need several common tools for this section. First, we will need to cut away some of the plastic wrap in back with a knife or similar tool.
Shown here are 3 tools, any of which can be used to cut out a rectangular section of plastic wrap behind the canvas: an "X-Acto" style knife, a pocket knife and a ceramic blade like this Slice Craft Knife carried by Adafruit.
Choose your weapon and then cut away the protective plastic in the rectangular section behind the canvas. This will allow for leaving the front protective plastic wrap on while attaching the hanging hardware in back.
Now that the protective plastic has been removed in back we can access the space just behind the canvas. Here I have opened up the hanging wire and D-rings. Curiously, the D-rings come in packs of 3. We will only need 2 D-rings for this. And there is enough hanging wire in this pack for many, many CompuCanvases.
Shown here are two more basic tools we'll need: a wire cutter to cut a section of the hanging wire and a Phillips screwdriver for the D-ring screws.
I'm not sure if there is an optimal place for the hanging wire, but I recommend placing it near the top, a few inches down. On this canvas the paper labeling extends down about 3 inches. I poke a starter hole with a screw, as shown in the picture, in the middle of the wood just below the paper.
Then screw in this D-ring and repeat the process of marking a spot and screwing in the D-ring on the other side of the canvas.
Now with both D-rings attached, cut a section of the hanging wire about 17 inches (my rule of thumb for this is to take the width of the canvas - 11 inches - and add 6 more inches to that).
I crimp the wire with my fingers to measure out the middle section. It's important to leave a little slack so it's not too difficult to hang on the wall, but don't leave so much slack that the wire is visible over the top of the canvas.
This series of pictures shows how I wrap the hanging wire around itself to attach it to the D-rings. Looping it around 7-10 times should be plenty to keep it on the wall, and you can cut away any extra hanging wire with the wire cutter tool.
Now, repeat the wire-looping exercise described above on the other D-ring and you will have a canvas that can hang on the wall!
Note in this picture how there is just about half an inch of slack in the hanging wire. It's not an exact science, but this is about right.
If you got the 8x10 inch foam board and offset clips for attaching parts behind the canvas, now is the time to add them. Get 2 of the offset clips with their screws ready for the next step.
Warning! When I took the original pictures here I thought the offset clips would be fine about 2.5 inches from the edge of the canvas. But midway through the next section, I realized that on the left side, this will interfere with one of the cables.
The additional pictures here show how I moved the left offset clip another inch toward the center. I also added another offset clip on the top right (see the final picture).
Note also that the holes here are little below the center of the wood frame, but not so low that it might break through the edge of the wood as it gets screwed in. For the offset clip on top, make sure to leave a little extra space so the foam board can easily slide in and out.
Now you have a blank canvas that hangs on the wall. Proceed to the next section to learn how to place a Raspberry Pi and other computer parts into the canvas assembly.
Computers on Canvas
At the end of the last section, we had a blank canvas that can hang on the wall, but with no electronics. The goal for this section is to end up with a canvas that is still mostly blank - allowing for an infinity of further design possibilities - but it will have a running Raspberry Pi system behind the canvas, with one wire bringing in both power and Ethernet.
These pictures show the end goal for this section. Behind the canvas is a running Raspberry Pi model 3B with a Power over Ethernet adapter and a USB speaker. The front of the canvas is still primarily blank, except for 4 small nylon screws holding the Raspberry Pi behind the canvas and the circular Ethernet jack.
Next, I will describe the parts and tools needed to build the Raspberry Pi system. Before I do that, I want to disclaim that I have some biases when it comes to building Raspberry Pi systems: I prefer Ethernet to WiFi and I like to use a rPi2B, rPi3B or rPi3B because of the 4 CPU cores and 1 GB RAM.
But there are a zillion ways to build a CompuCanvas! You could take a more minimal (pure WiFi) approach with a Raspberry Pi Zero W, or go even more minimal and build the system around something like a Circuit Playground Bluefruit. Or you could go bigger with something like a rPi4B. However, changes like that will necessitate other changes to parts and layout that I haven't considered here. So, you may want to continue following along with my selection of parts and steps.
The main picture here shows roughly how I will arrange the rPi system behind the canvas. The second picture shows the key parts (the PyRulers are just shown for scale).
The parts you will need with their Adafruit links are listed just below.
Note that we will use some parts from the nylon screw and standoff set in this section and then use more parts from this set in later sections.
Also, you will need a microSD card for the Raspberry Pi filesystem and you may need an adapter to write a Raspbian image on the microSD card. In case you don't already have these parts, the links are just below.
The parts above will be placed inside the canvas (except for the USB microSD card reader/writer, which is a tool used for programming the microSD memory card). There are some additional parts you will need, to bring power and Ethernet into the canvas.
I like the way that flat Ethernet cables drape from the front of the canvas down to the floor, so I look for cables like the one shown here. This one is seven feet long, but you may need something longer depending on how you place the CompuCanvas in a room.
The other part here is a Power over Ethernet (PoE) injector. This will take power from a wall plug and Ethernet from your home router as input and send out PoE. You don't need the specific TrendNet part shown here, but you do need to use an IEEE 802.3af PoE injector to be compatible with the PoE splitter from the parts list above.
I couldn't find these parts at Adafruit, but they (and similar/compatible parts) are available from many online sources.
There are a few more parts and tools you will need for this section. For most of these, the hardware store is where you will likely find them.
The pictures here show hardware parts that I have used to attach cables to the wood frame of the canvas. I recommend the style of staples shown on the right, if you can find them. These can be pressed in with your thumb such that they will hold temporarily while you layout the parts. Then you can hammer them in more later when your layout is certain.
You will only need 2 or 3 of these staples for this project, so don't buy everything you see here! Just one pack will be enough.
This picture shows some additional tools you will need. The hammer, shown on top, is used for final placement of the cable staples discussed above.
Shown on the lower left here are needles and awls which I use to poke small holes in the canvas. Adafruit sells a needle set, but I have also collected some other needles which are a bit larger. I often start by poking a hole with one of the needles to mark a spot and then use one of the awl tools to make the hole large enough for the nylon screws discussed above.
On the lower right are blades for making straight cuts or large rounded cuts in the canvas. These were already introduced in the previous section of this guide.
Finally, I use a mechanical pencil to mark spots on the canvas for cutting or poking holes. And the PyRulers shown here are not just for scale! You will want a ruler around to measure for some of the layout activities.
Now, with all of these parts and tools assembled we can get down to business. The next few steps will show how I arranged the computer parts behind the canvas and started to mark spots to cut through the canvas.
I'm going to start by laying out the panel mount Ethernet cable. The pictures here show how I removed the circular piece that holds the cable from behind and used it to trace out a circle where I will cut through the canvas.
Some other things to note here:
Here I am preparing to mark 4 spots to poke holes for mounting the Raspberry Pi to the canvas. The key things to note are:
When arranging computer parts on these art canvasses, be careful not to place any of the chips that may get hot directly against the canvas. Some of the chips on the Raspberry Pi can get quite hot. The design I present here leaves plenty of air gap between the hot parts of the rPi and the canvas.
Now, hold the Raspberry Pi down in the exact spot where you want it on the canvas and use a mechanical pencil to mark the 4 mounting holes, as shown in the second picture here.
I find that I have to extend the lead from the pencil much more than I would for writing on paper to allow it to reach the canvas. This means it can break easily. But you don't need dark marks for this. Just gently circle the pencil around in each mounting hole and you should get clear enough markings for the next step.
Now it is finally time to make some cuts in the canvas!
First, use a blade type tool to carefully cut around the circle you traced for the Ethernet cable.
Next, use a needle to poke through the center of each of the 4 rPi mounting holes. We will make these holes larger (with the awl) in an upcoming step. For now, you just need holes that are visible from the front of the canvas.
The last picture here shows the canvas from the front. Note that the protective plastic is still (mostly) covering the canvas. If you peek ahead to the next step, you'll notice the protective plastic is gone. You know what that means! Yes, go ahead and rip off all the extra plastic to fully reveal your canvas!
Here I have threaded the Ethernet cable through the front of the canvas and screwed the plastic nut in back to secure it in place.
It was surprisingly difficult to turn the nut around with my fingers, so this step took a while. You may find that a pliers or wrench helps here, or just be patient and gently fiddle it around until it is flush with the canvas.
In the next step we will widen the 4 rPi mounting holes and place nylon screws through them. Here you just need to collect the nylon screw parts to use. The first picture shows how the nylon standoffs will be attached to the rPi. The second picture identifies which parts to use from the nylon screw kit, but you need 4 of each:
You can go ahead and attach the standoffs to your rPi as shown in the first picture here.
The 4 nylon screws need to be inserted through the front of the canvas now, so we can attach the rPi in back.
To accomplish this, I start by poking a needle through the holes in front and wobbling it around to make the holes a little wider. Then I insert the awl and gently twist and push to make the hole even wider.
Be careful not to make the holes too big! This step can take some time. I gently work on making the holes bigger until they reach the point where they are just wide enough to place the screw and use a screwdriver to twist it all the way in.
The next step is to secure the Raspberry Pi in place. Hold it up so the standoffs align with the screws and then use a screwdriver to attach each one.
Now I am positioning the USB speaker behind the Ethernet cable.
The speaker cable is much longer than is needed here. In the last picture, I've used a yellow twist-tie to attach the extra speaker cable to the Ethernet cable. This helps keep the speaker in place and keeps the extra cabling out of the way.
You will also need to plug in a microSD card with Raspbian, or your preferred OS.
As the pictures here show, the microSD slot is under the rPi on the bottom. It should be inserted with the traces facing toward you.
If you are not sure how to prepare the microSD, don't panic! The next section in this guide will cover the software side of getting your CompuCanvas up and running.
Now we're almost ready to boot this system up! The pictures here show how the PoE injector gets connected in front of the canvas. The yellow Ethernet cable connected to "DATA IN" needs to also be connected to a router or switch on the other end.
Ok, now take a deep breath and admire the pure, pristine beauty of your CompuCanvas enclosure. It's like the Beatles "White Album"! It's like a field covered with fresh snow!
But things are about to get messy. We've been doing physical construction, but now it's time to do software. The next section will cover details from how to setup a microSD card with Raspbian to how to find the CompuCanvas on your network, login, and do initial configuration of the system.
Digressions in Code
In this section I'll first show how to prepare a microSD card with Raspbian to boot on your CompuCanvas. Then I'll walk through some of the setup steps that I perform to configure a new system. If you already have your CompuCanvas running you can skip over the initial material here.
Preparing a microSD card with Raspbian
If you want to use a Windows machine or a Mac to prepare your microSD card, refer to this other learn guide about rPi setup. I noticed that guide does not show how to use a Raspberry Pi to do the setup. I often use one rPi system to prepare the microSD card for another, so I'll detail those steps here to complement the other guide. I'll be using a Raspberry Pi with a monitor, keyboard, and mouse connected to it. But these steps could be performed with a headless rPi (like a CompuCanvas) as well.
The first thing to do is download a Raspbian image... but even before doing that you should check to make sure you have enough room for downloading and unzipping one of these large files. You can use the df command to figure out how much free space you have. The screenshot below shows how I changed to the Downloads directory and then ran df -h . and that shows I have about 50 Gigabytes free (on a 64GB microSD card), which will be plenty.
As I write this, the Raspbian downloads page has 3 editions of "Buster". Any of them should be ok for running a CompuCanvas. I usually choose the medium sized one: "Raspbian Buster with desktop". It's ok to use the 'desktop' editions even though the CompuCanvas won't have a proper monitor setup.
The download I got is called 2019-09-26-raspbian-buster.zip. The size of this file is about 1.1 Gigabytes, but we need to unzip it (with the unzip command), and that will produce a file with the same name but a .img extension. This 'image' file is about 3.6 Gigabytes. So, I will need almost 5 GB of free space on my system to perform this operation. As shown in the picture above, I have plenty of space, but you should check this too before downloading and unzipping the image.
If you are working entirely from the command line, you can use the wget command to download the zip file, like this:
wget -O raspbian.zip https://downloads.raspberrypi.org/raspbian_latest
If you are using a browser, you can click the link and it will be downloaded to the /home/pi/Downloads directory.
In the picture below, I've downloaded two of the Raspbian zips and moved them to a directory named rPi that I created to organize them. I have also unzipped one to get the .img file that will be copied to the microSD card.
The next step will be to use a USB to microSD adapter, like the part from Adafruit that was introduced in an earlier section of this guide. We will also need a microSD card.
The pictures here show inserting the microSD card into the adapter.
Next, we'll want to plug this into the rPi system where we have the Raspbian image file. When we plug in the adapter, it should become visible as a device with a filename like /dev/sda, /dev/sdb or similar.
In the picture below, you can see I ran ls /dev/sd* before plugging in the microSD adapter. On the first run there were no files found matching that pattern. Then I plugged in the adapter and ran the same command again. Now I see a sda and sda1 files in /dev. The first one represents the physical device and the second is a logical volume on that device. If we had a second of these adapters plugged in, we would see /dev/sdb and some logical volumes on it matching the pattern /dev/sdb*.
Checking this is important, because the next step is to write the image file to the microSD card. Doing this will erase and overwrite any data on the device we write to, so it's really important to identify the microSD correctly before proceeding. My before-and-after test shown below is a good way of confirming the device name.
Now we can run the dd command to copy the image file to the microSD card. The magic command for this is shown just below. However, note that you will need to fix 2 things before running it. I used raspbian.img as the image file name, but you will need to replace this with the actual image filename from the zip download. Second, I used /dev/sdXYZ as an example device to write to. Replace this with the device we found in the previous step, which is probably /dev/sda, but I always double-check to avoid overwriting the wrong device.
sudo dd bs=64K if=raspbian.img of=/dev/sdXYZ status=progress ; sync
The sync command at the end is really important too! This makes sure that all the data gets written out to the physical disk (instead of being cached on the rPi) so that it will be safe to remove the microSD adapter.
These pictures show how I constructed the dd command and then ran it. The status=progress option gives feedback as the copy is happening, then a summary is printed when it finishes.
There is one more crucial step to perform before unplugging the microSD adapter. As a security measure, remote login (with the ssh command) is disabled by default on new Raspbian images. But remote login will be the primary way of controlling the CompuCanvas, so we need to enable it.
The method for enabling remote logins is to write a file named ssh at the top-level of the "boot" filesystem. But first we may need to mount the boot filesystem, so we can write this file to it. When we wrote the Raspbian image file to the microSD card, it should have created 2 logical volumes, a "boot" volume and a "root" filesystem. If you are lucky, they will get auto-mounted under /media/pi but I checked there and was not lucky, so I will need to manually mount the boot filesystem to write the ssh file on it.
The picture below shows how I ran sudo fdisk -l /dev/sda which prints some information about the 2 logical volumes (sda1and sda2) associated with the physical microSD card (/dev/sda). The device with "FAT32" in the type field is the boot volume that we need to mount.
We will need an empty directory to mount the boot filesystem. When things get auto-mounted, they appear under /media/pi. In the picture below, I created a directory /media/pi/microSD to use as the mount point. This will only need to be done once on this machine:
sudo mkdir /media/pi/microSD
Then I ran the following command to mount the volume:
sudo mount /dev/sda1 /media/pi/microSD
After this, as the picture shows, we can ls /media/pi/microSD and see a bunch of files that are used as the Raspberry Pi boots up.
Now I can create the magic ssh file that enables remote logins. This is accomplished with the touch command. which creates a new, empty file:
sudo touch /media/pi/microSD/ssh
The picture below shows the before and after running the command. Notice the ssh file is present the second time we check that directory with ls.
Finally, you should run the sync command one more time to make sure all information is written out to the microSD card, and then unmount the root volume with this command:
sudo umount /dev/sda
This is shown in the next picture
Now you can remove the microSD adapter from this Raspberry Pi and put it into the CompuCanvas!
We can now proceed to the next sub-section of this software odyssey.
Logging into a new CompuCanvas
When you power up the CompuCanvas and it starts to boot up, it will get assigned an IP address on your network. You'll need to find that IP address and use it with the ssh command to login from the second Raspberry Pi. One way to find devices on your local network is with the nmap command. You might need to install it first, like this:
sudo apt update
sudo apt install nmap
Home routers often assign IP addresses where the first 3 digits are 192.168.1 and the final digit is between 1 and 254. So, the CompuCanvas could pop up at an address like 192.168.1.33 or any one of about 254 other possibilities. With nmap you can search a range of addresses. You may need to adjust the IP addresses I show for your own network/router configuration. The command below shows how to scan for all devices under 192.168.1:
nmap -sP 192.168.1.1-254
Similar to identifying the microSD card, you'll want to run this command before plugging in the CompuCanvas and get a list of devices currently on your network. Then plugin in the CompuCanvas and wait a few minutes for it to start up and get an IP address assigned. Then run the same nmap command again and look for a new device and note that IP address for the next sub-section.
Suppose that your nmap command shows a new device at address 192.168.1.33 on your network. You can try to login with the ssh command like this:
ssh pi@192.168.1.33
Sometimes I see several new/unknown devices in the nmap output and I have to guess. If you try to login to the wrong IP address, you will probably see a "connection refused" message.
The pictures here show my initial login to the CompuCanvas. (Note that my subnet is actually 192.168.2 instead of 192.168.1, as reflected in these pictures).
My host rPi doesn't trust this unknown machine, and I have to confirm the connection is ok by typing yes at the prompt.
Then I get a login prompt. In these fresh Raspbian images, there is a pi user account and the default password is raspberry. My ssh command specified the userid (with the pi@... syntax), so to complete the login I just need to type the default password.
Initial system configuration
The first thing I do when logging into a new Raspbian system is change the pi account password from the default to something else. As shown in these pictures, you can change your password with this command:
sudo passwd pi
Then you need to type the new password twice to confirm the change. Please write down the new password in a safe place.
The next step I take in setting up a new CompuCanvas is to run the raspi-config utility. This command line tool can perform most of the initial configuration you may want for running the CompuCanvas on your network. To start this, type:
sudo raspi-config
The next series of pictures will show some of the features of raspi-config.
Some things to note about these pictures of the raspi-config utility:
After the first reboot, there is still a bit more setup to do. I login to the CompuCanvas again with ssh and then run these 2 commands:
sudo apt update
sudo apt upgrade
This will upgrade the Raspbian operating system packages to their latest versions. The second command may take a long time, and there may be prompts where you need to type something to make it proceed. The picture below shows the beginning of this process.
It is a good idea to reboot again after this upgrading, but first you could install additional software to run on the CompuCanvas. There are 2 utilities that we will use later in the guide: espeak and screen. You should install those now with the following command:
sudo apt install espeak screen
You could install additional software at this point as well. After that, reboot again:
sudo reboot
The final bit of system configuration will be setting up the audio, so we can hear sound from the USB speaker. Next, I'll transition back to physical construction topics - specifically lighting up the inside of the canvas.
Internal Lighting
In this section I'll show several different ways to place and control lights behind the canvas. I'll use the parts shown below as well as some more parts from the nylon screw and standoff kit.
The parts list above includes 2 different USB cables. I'll first show how to use the short USB cable and some of the nylon screw parts to attach an Adafruit NeoTrellis M4 board directly to the Raspberry Pi.
Later, I'll use the longer USB cable to show how you could instead attach the NeoTrellis M4 to foam board placed behind the canvas. This configuration will allow for more variability on positioning of the NeoTrellis M4.
From the nylon screw kit, pull out one of the medium size screws, a shorter size standoff and the longest of the straight spacer pieces. Read on to see how these will be attached to the Raspberry Pi.
Here I am screwing the spacer part into the upper left of the 4 nylon screw assemblies holding the Raspberry Pi.
Now screw the standoff on top of the spacer as shown in these pictures.
In these pictures, you can see how I've connected the NeoTrellis M4 to the short USB cable and then plugged that into one of the USB ports in the Raspberry Pi.
At this point, the NeoTrellis M4 is hanging freely, but in the next step I'll show how I oriented it over the Raspberry Pi and then attached it with the nylon screw.
You'll probably need to massage this USB cable a bit to get these parts to hang well together.
Notice in these pictures how I've placed the nylon screw through the hole near the SDA and SCL markings on the board. But if your cable is a little longer or shorter, you may find that another mounting hole works better.
At this point we can boot up the Raspberry Pi system and use the screen utility to connect to the CircuitPython REPL on the NeoTrellis M4.
Usually the first connected CircuitPython device will be represented as /dev/ttyACM0 on the Raspberry Pi, and you can connect and talk to the REPL with this shell command:
screen /dev/ttyACM0
If this REPL connection is working, you should be able to press Enter (or use Control-D to reset the board) and see a >>> prompt allowing Python commands to be entered. If there is a Python program running, you can use Control-C to stop it. To end the screen command session, type Control-A followed by the K and Y keys.
I used the adafruit_trellism4 library to control the lights on the NeoTrellis M4 through the REPL. This required copying several libraries from the Adafruit library bundle. I downloaded the library bundle from the CircuitPython site and unzipped it, and from the lib directory in there I copied 3 of the .mpy files to the NeoTrellis M4 drive as shown below:
cp adafruit_trellism4.mpy /media/pi/CIRCUITPY/lib ; sync
cp neopixel.mpy /media/pi/CIRCUITPY/lib ; sync
cp adafruit_matrixkeypad.mpy /media/pi/CIRCUITPY/lib ; sync
... now with that all ready, use screen to connect to the REPL. In the REPL, first do Control-D and then press Enter a few times and look for the >>> prompt. Then issue these commands:
import adafruit_trellism4
trellis = adafruit_trellism4.TrellisM4Express()
trellis.pixels.fill((0,0,128))
After doing this, my CompuCanvas looks like the picture below.
In the picture here, I have just one of the NeoPixels emitting green light and the rest are off. To get to this state, I first used this command in the REPL to turn all the NeoPixels off:
trellis.pixels.fill((0,0,0))
Then, I set a single NeoPixel like this:
trellis.pixels[0,0]=(0,128,0)
Note that this NeoTrellis M4 board has 32 NeoPixels in an 8x4 grid. So one corner can be addressed by trellis.pixels[0,0] and the far corner is trellis.pixels[7,3].
To get the picture here, I turned the lower left NeoPixel blue with this command in the REPL:
trellis.pixels[0,3]=(0,0,128)
For this picture, I have illuminated the other 2 corner NeoPixels with the following commands:
trellis.pixels[7,0]=(0,0,128)
trellis.pixels[7,3]=(0,128,0)
I've found that a lot of interesting things happen when the lights are just behind the edges of the other parts. For these pictures, I first cleared all the NeoPixels:
trellis.pixels.fill((0,0,0))
Then I set 4 of them that seem to be aligned just behind the Raspberry Pi with the following:
trellis.pixels[0,0]=(0,0,128)
trellis.pixels[3,0]=(0,0,128)
trellis.pixels[0,3]=(0,128,0)
trellis.pixels[3,3]=(0,128,0)
I like how the spikey shadows from the expansion pins are visible on the right side of the Raspberry Pi with this illumination pattern.
Ok, now let's try something completely different! What if we move the NeoTrellis M4 off of the Raspberry Pi and instead attach it to the foam board?
Before we get to that, I'll first go over this series of pictures that show how I fine-tuned the foam board to fit with the other parts behind the canvas.
The Ethernet cable is just deep enough that it blocks the foam board from fitting in place.
The quick and easy solution to this kind of problem is to just cut away a bit of the foam board. The pictures here show how I - with a bit of trial and error - cut enough to allow the foam board to rest squarely against the offset clips attached to the bottom of the canvas.
In these pictures I'm sizing up how to position the NeoTrellis M4 on the foam board. I used the mechanical pencil to mark spots aligned with 2 of the mounting holes on the NeoTrellis M4. Then I used the awl to cut holes through these marked spots to fit the nylon screws.
From the nylon screw set, pull out 2 of the hex nuts, 2 of the longest screws and 2 of the shorter standoffs. The pictures here show how I attached the standoffs at the points I marked on the foam board in the previous steps.
Note that the last picture shows how the standoffs can end up very close to some of the electronic parts. Be careful not to twist the standoffs too much against these surface mounted parts!
In these pictures I threaded the nylon screws through the holes in the foam board. Then I mounted the NeoTrellis M4 on the foam board as shown.
Now the foam board can be fit into the offset clips behind the canvas. It's a snug fit, but everything has a place.
In these pictures I am testing the look of this new positioning of the NeoTrellis M4. As in the earlier examples above, I am using the screen command to connect to the REPL and issuing commands like shown below to light all the NeoPixels with one color:
import adafruit_trellism4
trellis = adafruit_trellism4.TrellisM4Express()
trellis.pixels.fill((0,128,0))
Here are some more lighting tests with the new NeoTrellis M4 positioning. In this orientation the NeoPixel at coordinate [0,0] is on the lower left, and [7,3] is in the upper right corner.
Continue to the next page to see an alternative approach to placing light behind the canvas.
Alternate Internal Lighting
In this section I'll show a different way of illuminating the back of the canvas using the parts shown above, which are also listed just below. The primary part is a NeoPixel strip with 30 RGB LEDs. This will be controlled by a Gemma M0. A USB cable is needed to connect the Gemma M0 to the Raspberry Pi. Finally, another piece of the 8-inch by 10-inch foam board will be used to secure these parts behind the canvas.
Before getting into the weeds of this section, I want to stress a few points about this approach to interior lighting:
In these pictures, I'm trying to show that the NeoPixel strip will occupy a bit more depth behind the canvas than the NeoTrellis M4 does. When arranged on the foam board, it needs to avoid obstructions like the PoE adapter, the speaker, and the USB and Ethernet ports on the Raspberry Pi.
These pictures show how I use the foam board setup from the last section to trace out where to cut the new foam board for this section. The previous cut was a bit gnarly, so I rounded out my trace and then made the cut and checked that the foam board does indeed fit behind the canvas.
This series of pictures shows how I've tried to map out the canvas interior to identify where the NeoPixel strip can be placed. There is quite a bit of eye-balling and fuzzy logic to this process....
Here I'm starting to attach the NeoPixel strip to the foam board. I'm going to use the twist-tie that came with the USB cable. You could also use bits of wire or small zip ties for this.
Note how I'm using the awl to poke holes in the foam board and then threading the twist-tie through the foam board and around end of the NeoPixel strip.
As I go forward here, I'm trying to keep the NeoPixel strip inside the lines I've marked on the foam board. In some cases, my initial mount points didn't work, so I poked more holes and re-positioned the NeoPixel strip. The foam board can withstand a lot of damage and is relatively inexpensive, so buy a few extra pieces and don't fear about experimenting with alternate configurations.
I actually have a collection of these twist-ties, saved from the purchase of many cables and other assorted things. Here I've selected a range of colors and I'll place them at different points to hold the NeoPixel strip to the foam board while avoiding obstructions of parts attached to the canvas.
Bits of stiff wire can also be used.
The first picture here shows how I ultimately connected the Gemma M0 to the foam board and the NeoPixel strip. The additional pictures show how I got to this point, measuring, marking and using the nylon screw parts to mount the Gemma M0 on the foam board.
Note that the Gemma M0 is connected to the NeoPixel strip alligator clips as follows:
See also this NeoPixel page from the Gemma M0 guide which shows a wiring diagram and has a CircuitPython code example.
Here I am fitting this interior lighting setup onto the back of the canvas.
In these pictures I've booted up the system and am testing the lights. In the first picture, the green light is the NeoPixel at index 0. The rest of the NeoPixels on the strip are blue. The pinkish light is the DotStar on the Gemma M0.
To control these lights through the CircuitPython REPL, you will need code something like this:
import board, neopixel
pixels = neopixel.NeoPixel(board.A1, 30)
pixels.fill((0,0,200))
pixels[0]=(0,200,0)
Due to the orientation of the NeoPixels, this is a more subdued lighting style than shown in the last section, but it covers more of the canvas interior.
External Features
In the previous sections, I've placed parts inside the canvas to create lighting effects emanating from the interior. In my experience, the most interesting lighting effects come from placing lights on both sides of the canvas, with interior lights directed out and exterior lights pointing back onto the canvas.
In this section I am going to show some ways of transitioning from behind the canvas to the exterior such that light may be directed at the front side of the canvas.
I want to stress here that I've left the front of the canvas plain up to this point in the guide because you may arrive at better, cooler, more stylish exterior designs than I can imagine. As I proceed, my general design idea is to make it look like flowering plants are sprouting out of the canvas. You may want to read ahead and then consider whether you want to follow me exactly or branch out with a different set of parts and designs for the front of your canvas.
The key part I've chosen for transitioning from the back to the front of the canvas are the USB panel mount cables shown here (and in the parts list just below).
In the pictures here, I am sizing up roughly how the cables will sit on the back of the canvas.
I'll add these cables one at a time. After seeing my results, you may choose to do only one or the other, or to find some other arrangement and set of parts.
What follows next is the parts list and process for adding the first external feature: A Circuit Playground Express. In the next section, I will show how to mount a Gemma M0 as a second external feature.
These pictures show roughly how the parts will be arranged from the front. In the second picture, the panel mount USB cable is oriented horizontally, which makes the ribbon cable flat. As you'll see in upcoming pictures, I chose instead to orient the panel mount USB cable vertically, which gives the ribbon cable a twist.
In this picture I have the CompuCanvas running, but turned around and resting against the wall. I have the exact cable assembly I plan to use, and I've confirmed that I can access the CircuitPython REPL and control the NeoPixels.
This type of test is advisable before committing these parts to the canvas. In fact, the first cable assembly I tried did not work. The ribbon cables can be tricky to assemble! I ended up swapping a few parts (I was originally trying to use a 10 cm ribbon cable) and then was able to confirm the configuration shown here worked.
In these pictures I am measuring and marking a rectangle where I will cut a hole for the USB cable. Some things to highlight about this process:
In these pictures, I show cutting the rectangular hole in the canvas and the beginning to place the USB cable.
One thing to double-check is the orientation of the USB cable. It could be flipped in one of 2 directions. The last picture shows how I plugged in the Circuit Playground Express to make sure this orientation of the USB cable works.
In these pictures, I have pulled the USB cable into place. The sides of the USB cable have plastic prongs that bend a little as the cable slides in. I try to push the prongs in as I pull the cable through and then wiggle the cable a bit to nest it in place.
In the back, notice how the cable needs to be massaged away from where the foam board (or wall) will be.
These pictures show how I marked 6 spots on the canvas where I will poke holes to attach the Circuit Playground Express (CPX).
You may notice a lot of the nylon screw parts attached to the CPX in these pictures. This arrangement will be explained just below.
You may also notice that I 'cheated' when marking these spots by using a second CPX. If you have a second CPX, you can skip ahead and attach the nylon screw parts and then mark things the way I did. If you just have the one CPX, try to find and mark a place where it will hang well before attaching the nylon screws.
Either way, if you are following my lead here you should mark these 6 spots:
In these pictures, I'm starting to attach a bunch of nylon screw parts to the Circuit Playground Express.
First, I attached 6 of the longest standoffs at the points shown. These 6 standoffs will be used to mount the CPX to the canvas, so they correspond to the 6 points marked in the previous step.
I actually ended up using the last 6 of the longest standoffs from the kit for this (I had to reclaim one from the Gemma M0 used in the alternate interior lighting setup). If you run out of long standoffs, 2 of the shorter standoffs are about the same length.
These pictures show how I also attached some of the nylon spacer parts to the CPX.
These are not for attaching to the canvas. Instead they should enhance the "light-show" by both capturing some of the light (and glowing) and also blocking some light, creating shadows on the canvas.
There are lots of variations that could be explored using the nylon screw parts to tune the NeoPixel light from the CPX.
In this step I poked through the 6 spots in the canvas where I'm going to mount the Circuit Playground Express. I used the awl widen the holes just enough to screw the standoffs through the canvas.
I had to detach the standoffs from the CPX initially here. The pictures show how I used 6 of the nylon hex nuts to attach the standoffs to the canvas. Finally, I placed the CPX on the front over the standoffs and screwed it in.
In these pictures, I've booted up the system and tried a few different light configurations. Once you get into the REPL, use commands like this to control the NeoPixels:
import board, neopixel
pixels =
neopixel.NeoPixel(board.NEOPIXEL, 10)
pixels.fill((0,0,30))
pixels[0]=(0,60,0)
These pictures show how I re-attached the NeoTrellis to the Raspberry Pi using the short USB cable. This time I used one more of the short nylon standoffs to avoid the NeoTrellis M4 from contacting the USB panel mount cable.
Here I am testing the lights on both the Circuit Playground Express and the NeoTrellis M4 to find combinations that look nice.
At this point we could declare this CompuCanvas finished from a hardware point of view and refocus on creating animations for the lights or other programming exercises. But read on if you want to see how I placed another feature on the front of the canvas using a different type of cable assembly.
More External Features
One of the tricky things about making transitions through the canvas is finding cable parts that make right-angle type turns on each side. The ribbon cable system I showed in the last section may be the best set of parts Adafruit currently offers for these right-angle USB cable turns.
But another way of making right (or left, or up, or down) cable turns is to find (or fabricate) a custom cable with the desired length and orientation.
This picture shows a whole bunch of USB cables I have collected that have various styles of right/left/up/down turns.
You can find these at sites like Amazon by searching for "short left right angle micro USB cable" or similar. These often come in pairs with both the "left" and "right" versions. I look for the pairs because it's sometimes hard to figure out which of the two I will need until I have them in hand.
I am going to use one of the "angled USB adapters" shown here - whichever one happens to angle the way I want.
In addition to one of the USB adapters shown above, I will use the following Adafruit parts. You may already have some of these from the earlier experiments in interior lighting. If so, you can repurpose them here as I did.
These pictures show the parts described above. As with the CPX, I tested the full cable assembly for the Gemma M0 before committing any of it to the canvas.
Here I measured and then cut another 1.1 by 1.9 cm hole in the canvas. I'm placing this one a little lower than the other. As before, I've checked both side of the canvas to make sure the cable will not bump into anything on the inside.
These pictures show how I've snapped the panel mount USB cable into the canvas - after making sure the orientation of the cable works with the USB adapter I chose.
Then I connected the cable assembly with the Gemma M0. This is another situation where I needed to do a lot of "cable massage" to get the short USB cable into the curly shape you can see here.
I think one set of the nylon screw parts will be enough to keep the Gemma M0 attached to the canvas. These pictures show how I marked a spot on the canvas to attach the Gemma M0 through the hole near the 'A' in 'GEMMA' on the silk screen.
Now we can try out lighting tests with the DotStar RGB LED on the Gemma M0. See this Gemma M0 guide page for all the details. You may need to first copy the adafruit_dotstar library to your Gemma M0. With that library you should be able to see some color from the DotStar in the CircuitPython REPL with commands like this:
import adafruit_dotstarled =
adafruit_dotstar.DotStar(board.APA102_SCK, board.APA102_MOSI, 1)
led[0] = (80, 0, 80)
Here I will once more attach the NeoTrellis M4 to the Raspberry Pi using the nylon screw set. The first picture shows both USB cables, but I will only use the longer cable for this.
I want the NeoTrellis M4 to sit vertically, behind the rPi and the USB cables sprouting out of it. Note that I am connecting to a different corner of the rPi than in previous instances where I mounted the NeoTrellis M4.
I threaded the USB cable for the NeoTrellis M4 through the USB speaker cable and then arranged it so the extra cabling rests on the bottom of the canvas frame, as shown here.
This picture shows what it looks like when you boot a Raspberry Pi with 3 CircuitPython devices attached.
Note how we can print out the boot_out.txt files to see which of the CIRCUITPY directories corresponds to which device.
Also note how we have the 3 ttyACM devices in /dev. I don't know how to tell which is which other than using screen to connect to the REPL of each one.
Here I am conducting light tests with all three CircuitPython devices.
I am now going to declare this CompuCanvas finished from a hardware point of view. The Python light show code could be tweaked endlessly, but I will leave that as an exercise to the reader.
Here are several more pictures with different lighting configurations.
Now with the physical construction of this CompuCanvas finished, we are almost at the end of this guide.
But there is one loose end to return to: the configuration of the USB speaker. The next (and final) section will detail how to test and configure the USB audio.
Audio Addendum
Raspbian comes with a command called speaker-test which is the first thing I try when setting up audio. The picture below shows what it looks like with the audio correctly configured. More importantly is what it sounds like! If everything is working, you will hear static ("pink noise") from the USB speaker. After listening for a while you can press Control-C to end speaker-test.
So, you might get lucky and find that your speaker just works, without any tweaking. I was not so lucky. When I initially ran speaker-test, it exited immediately with an error (and there was no sound).
If your speaker is already working, skip ahead to where I talk about the espeak command. Otherwise the next several steps will cover how I diagnosed and fixed the audio issue.
I found this StackExchange writeup about ALSA to be very helpful. One thing it recommends is looking at the files /proc/asound/modules and /proc/asound/cards. The picture below shows how I used the cat command to print out the contents of those files.
The picture above shows that 5 audio devices were detected! Why is this? Apparently CircuitPython devices register as audio devices, and in my case the first 3 devices listed are the NeoTrellisM4, the Gemma M0 and the CPX.
The device with index 3 is the real USB speaker. The last device ("bcm2835") is the audio system inside the Raspberry Pi which uses the rPi headphone jack.
The first device listed will be the default audio device, so in my case Raspbian was initially trying to use the NeoTrellis M4 as the speaker (and this failed speaker-test).
Another way to check the audio configuration is with the alsamixer command. The pictures here show that when I first ran it, the "Trellis M4 Express" card appeared first.
The second picture shows how you can press F6 to switch to a different sound card.
The final picture shows how I selected the USB speaker. This allows for controlling the volume (set at 50 in the picture) with the up and down arrow keys.
You can change the volume here and Raspbian will continue to use that setting after you exit alsamixer. However, we cannot change the default sound card from here. I'll show how to do that in the next step.
In the above steps, I determined that my USB speaker is the device with index 3 in /proc/asound/cards. By default, Raspbian is using device 0 (the NeoTrellis M4). So, I need to change the default value from 0 to 3... but where?
The answer to that question was in the StackExchange link. We can change the default audio card by editing this file: /usr/share/alsa/alsa.conf. This file is owned by the root user, so we need to launch an editor with sudo. You could do it with the nano editor like this:
sudo nano /usr/share/alsa/alsa.conf
Two lines need to be changed in the alsa.conf file. Look for these 2 lines:
defaults.ctl.card 0
defaults.pcm.card 0
The picture below shows how I changed those values from 0 to 3 because my USB speaker was assigned to audio card 3.
After changing the 2 values in the alsa.conf file, reboot to allow the changed settings to be processed:
sudo reboot
After this reboot, try the speaker-test command again and you should hear some noise from the speaker. You can run alsamixer again to adjust the volume.
Now, with all that setup done try this from the command line: espeak hello
You should hear your CompuCanvas say, "hello". You will also see a lot of error messages in the terminal window. If you are hearing sound, it's safe to ignore these messages. You can hide them in your command line invocations like this:
espeak "hello world" 2>/dev/null
The last bit (2>/dev/null) hides the error messages by sending them to the /dev/null device (sort of a digital trash can).
Below is a bash script I wrote that you can use to have your CompuCanvas announce itself and its IP address.
Download: file
#!/bin/bash
function espeaker() {
espeak -a 50 "$@" 2>/dev/null
}
IP_ADDR=`hostname -I`
while [ -z $IP_ADDR ]; do
sleep 1
IP_ADDR=`hostname -I`
done
ESPEAK_IP_ADDR=`echo $IP_ADDR | sed -e 's/\(.\)/\1 /g' | sed -e 's/\./dot/g'`
espeaker "Hello from Comp U Canvas"
sleep 2
espeaker "I P address"
espeaker -s 100 "$ESPEAK_IP_ADDR"
sleep 2
espeaker "repeating I P address"
espeaker -s 100 "$ESPEAK_IP_ADDR"
To try this out, use an editor to create a file for the script:
nano ~/cc-hello.sh
This will open nano on a new file named cc-hello.sh in your home directory. You can paste the above script into that file and save it. Then run the following to make the file executable:
chmod ugo x ~/cc-hello.sh
Now try to run the script:
~/cc-hello.sh
The ~ in the commands above refers to the user's home directory, which is /home/pi. So, the full path of this script is: /home/pi/cc-hello.sh. I'm going to use that in the next (and final) step of this guide.
The last thing I want to show is how you can make the cc-hello.sh script run when the CompuCanvas boots up. This is useful when taking the CompuCanvas to a new place (like a meetup), because you will need the IP address to login to the CompuCanvas.
There is probably more than one way to tie cc-hello.sh into the Raspbian boot sequence. I do it by editing the file /etc/rc.local. That file is owned by the root user, so you'll need sudo to edit it, like this:
sudo nano /etc/rc.local
Notice that the very last line of this file has exit 0. Add the line shown below just before the exit 0 line:
/home/pi/cc-hello.sh
Then save the changes, and sudo reboot one more time. When the CompuCanvas starts up again you should hear it announce its IP address.