Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
LTSPICE-Slide13

One or several NTC sensors and their associated Thermal Transfer functions can be introduced in any application. For this example a TEMPERATURE RATE of RISE detector has been chosen. The principle of a heat detector compares the signals given by two NTC sensors which have a different time response to a given rise of temperature. As the number of components in the circuit increases, so do the component tolerances (electrical and thermal), so it is best to perform a Monte Carlo Analysis rather than a Worst Case Analysis (N tolerance factors would require 2^N runs!).

PTM Published on: 2016-06-28