Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
LM5017 Synchronous Buck Converter and COT Slide 19
In summary, the TI LM5017 is the industry’s first 100 V synchronous buck converter with integrated FETs. TI has manufactured constant on-time (COT) high-voltage devices for a number of years which required an external catch diode. The LM5017 has a more integrated solution that is fully synchronous, more efficient, smaller, and more user-friendly. Two FETs are integrated in the IC as well as a high-voltage, 100 V startup regulator that biases all internal circuitry. A COT device is similar to a hysteretic device except there is an added block referred to as an on-timer. The COT control circuit maintains regulation by triggering the non-resettable on-time, which turns on the high side FET when the output voltage decreases to the lower threshold. The output voltage rises during the on-time. When the timer expires, it will turn off the switch and the voltage will fall again. Some of the benefits of the COT solution are constant frequency control, lightning-fast transient response, no loop compensation required, and it is simple to design with.
PTM Published on: 2012-04-26