Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Microstepping Stepper Motor Controller Slide 19

In summary, this presentation has introduced the L6470 stepper motor controller/driver IC. The L6470 includes a digital core that controls the motion profile along with the power bridges and the microstepping controller. The advantages of the L6470 include simplified design, reduced loading on the microcontroller, and smoother operation for the motor. It communicates with the microcontroller using an SPI interface. Configuration information and movement commands are sent to the L6470 across the SPI and the device sends status and fault information back to the microcontroller. A key feature of the L6470 is the dSpin core that implements a motion control algorithm in the dedicated state machine. Additional information on the STMicroelectronics L6470 and its operation can be found at www.st.com.

PTM Published on: 2013-01-22