Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 25

The load driven by an industrial IPS is often a low current. The L6374 has the lowest current of the portfolio, with a current of 100 mA and a current limit of 200 mA in the event of short circuit.

PTM Published on: 2011-09-07