Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
PZA-Slide12

The last application pertains to a phenomenon in the audio community known as phantom power. It is a method of transmitting DC electric power through microphone cables which is a convenient power source for condensing microphones. The low impedance 63V capacitor was typically a liquid type until now. Now this process can be satisfied with a high performance polymer cap instead which makes it suitable for the 48V filtering required by this circuit.

PTM Published on: 2014-05-05