Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
PZA-Slide10

The next few slides show typical applications using the PZ cap technology. The first is a high-speed IGBT. The circuit reaction rate assists to speed-up, lower the ESR and allow for high ripple current. The application example is for an IGBT gate drive used in an industrial application. A 35V PZA is suitable for a 15VDC line of an IGBT gate drive circuit.

PTM Published on: 2014-05-05