Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Pt2-Slide16

Now that the post-scalar is selected all we need to specify is the divisor value to obtain the 120MHz from the VCO. To get 120MHz with a 2MHz input, the VCO divisor must divide by 60. Now we have all of the parameters needed to program the VCO.

PTM Published on: 2011-11-07